Other Parts Discussed in Thread: BQ8050,
Tool/software:
Dear Ti engineer
If there will be a deviation in the wake-up cycle of the watchdog under low temperature conditions?
Best wishes
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are not aware of any deviation in the wake-up cycle of the watchdog under low temperature conditions.
Can you please elaborate the issue?
Hello,Jose
Now we have a sleep setting for 1S wakeup to be used as a sleep timing, this timing is very accurate at room temperature, but at -20℃, the timing error can be -14% to -15%. So we're guessing that's maybe the reason. What do you think
Best wishes
Hi Couso:
Could you please help to answer it when it is convenient for you? Thank you!
Best Regards,
zehu
Hello,
Hello,
Thank you very much for your earnest reply. I feel very honored
According to the user manual, it looks like we set the programming step size is 7.8125 ms, but we don't see where the error range of this 7.8125ms is explained,where can I find it?

Best Regards,
zehu
Hello,
Hello,Jose
I found the 32.768kHZ Oscillator perameters in the user manual, the 7.8125 ms step size has a -1.5% to +1.5% error at -20℃.It seems that the error in our test data is much large than in the user manual.

Is the error of 32.768kHZ Oscillator we found correct? Why is the difference so large?
Best Regards,
zehu
Hello,
Your observed 14–15% timing error corresponds to a 16.27–17.64% frequency error in the 32.768 kHz oscillator, which is consistent with your test data.
to +1.5% frequency error at −20C, but your observed error (16.27–17.64%) is much larger. Possible reasons include environmental factors (e.g., voltage, humidity) or test setup issues.