Tool/software:
Hi TI Expert,
Please refer to below SCH for TPSM861257, our customer would like to adjust the output(original is 3.3V) to 3.7V.
The recommended RFBB=30kOhm based on the datasheet's table 8-2 as below for the output of 3.3V/5V, take the same resistance value of RFBB for 3.7V Vout calculation, the standard resistance can be selected in the range of 154kOhm(Vout=3.68V) to 158kOhm(Vout=3.76V) for the RFBT(R315). Would you please let us know if the RFBT resistance value in the range is suitable as recommended?
Look forward to your feedback soon, thank you.
TPSM861257 RFBT & RFBB location and recommended component value table :