This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ500511: Wireless Power Transfer

Part Number: BQ500511
Other Parts Discussed in Thread: BQ500215

Tool/software:

Hello,

We have a requirement as below.

We have two units say A & B. Both are mounted on the same mechanical shaft with a metallic bearing between them. Both units are 10 cm apart. Module B has a battery of 10000 mAh whereas module A has a rechargeable battery of 80 mAh. Before the start of the operation, the power is to be sent from B unit to A unit wirelessly. Then the A units starts working.

Can we use BQ500511/ BQ500215? IS Wireless Power Transfer is possible between B & A unit to a distance of 10 cm.

Let me know.

If  BQ500511/ BQ500215 are not suitable, can you suggest alternate?