Tool/software:
Hello,
I am using LMR38010 buck converter for generating 12V from 48v as a part of power supply designs for my board. I want to understand the conditions where the transition to PFM and forced PWM happens from the normal PWM operation. I have seen the datasheet/application note but it is not very clear there. I have few basic questions below :
1. When will the transition between different modes happen exactly ?
2. If I have to change the transition point as above, say at different values of currents of my choice, what should I change in the buck converter design (inductor, capacitor, switching frequency ,etc) and how ?
3. Sometimes when I decrease the value of inductor then the point at which the DCM or I must say the PFM operation happens occurs at lower value of current compared to a higher value of inductor. How is this possible ?
4. Please suggest corner cases for the above. I need my converter to function in CCM above 0.15-0.2A load current atleast.
Please reply soon.