Other Parts Discussed in Thread: BQ25180, BQ25186
Tool/software:
Hi, in my application I have a battery with internal 10k @ 25°C NTC resistor connected to a BQ25185. The NTC has the same temperature profile as the 103AT-2 suggested here: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1308117/bq25185-how-to-select-the-correct-ntc-for-battery-temperature-monitoring
During temperature tests we noticed that the charge is interrupted @ 55°C but the battery can be charged only in the range 5°C - 45°C. The threshold voltage at TS pin when charge is interrupted correspond to the Vhot indicated in the datasheet, so looks like the BQ25185 is ok.
My question is: what is the temperature range where the BQ25185 allows the battery charging? If I need a different range, how can I adjust the circuit in order to meet my temperature requirements?
Thanks in advance
Alberto