This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521815: Intelli-PhaseTM Solution Replacement

Part Number: TPS6521815
Other Parts Discussed in Thread: TPS53631

Tool/software:

Dear Team,


Do you have Intelli-PhaseTM Solution parts that can replace MP87440 and MP87420?

A cross-reference search couldn't yield any part numbers.

BR,

  • Hi Hiroshi-san, 

    Are you able to give more details on the desired specifications?
    MP87420 does not appear to have any public information.

    Best Regards, 
    Sarah

  • Sarah san,
    Thanks for your confirmation!

    Do you have a similar product with the following specifications?
    I apologize for the lack of information.

    Product Type:half-bridge gate drivers with MOSFETs, Current sense, and temperature sense.
    Operating Input Voltage (VIN):22V
    Output Current (IOUT):30A

  • Hi Hiroshi-san, 


    I am reassigning your thread to another team who handles the half-bridge gate drivers, and may have a better idea of a similar product.
    Thank you for your patience!

    Best Regards, 
    Sarah

  • Hey Hiroshi,

    It seems that you need a half bridge driver with integrated power MOSFETs. I am with the discrete gate driver team and so I will transfer to the integrated power module team.

    Thank you,

    William Moore

  • Hiroshi-San,

    Are you looking for a motor driver device?

    Regards,

    -Adam

  • Sarah san, William san, Adam san,
    Thanks for your confirmation!

    Adam san,
    I'm looking for a half-bridge gate drivers with MOSFETs, Current sense, and temperature sense.

    BR,

  • Hiroshi-San,

    We offer a single half bridge gate driver with integrated current sense, but not integrated MOSFETs.

    Our Brushed and Stepper group also offers some drivers that may fit your needs.

    What type of motor or load are you driving?

    Regards,

    -Adam

  • Adam san,

    Thanks for reply!
    It is difficult to communicate this due to confidentiality considerations,
    but what I'm looking for is a “Vcore Power Management System Solution”.
    A similar product might be TPS53631, for example.

    BR,

  • Hiroshi-San,

    This device is within our MPP group, I am assigning your post to them for more direct support.

    Regards,

    -Adam

  • Hi Adam
    Thanks for sending this our way. This looks to be in our purview. 

    Hello Hiroshi-san
    I want to make sure I understand what you need, my team offers step-down power-stages (gate driver + MOSFETs for voltage regulation) and controllers (provides monitoring, diagnostics, and PWM control of power-stages) for server applications. 

    The MP87420 and MP87440 you mentioned look to be power stages, and the TPS53631 you referenced is a controller for powerstages. We do offer some competing products of the MP devices, but we may need to get into more detail to make sure we can find the most appropriate device for your application. 

    If you are worried about confidentiality, we can also continue this conversation via email so it's not being published on a public forum and we can speak more freely. Would you like to continue this via email? 

    Kind regards,
    Nick