This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM70880: Pspice for TI - Simulation failed

Part Number: LM70880

Tool/software:

Dear TI

I am designing a circuit using a LM70880 with the following specifications.

   Vin: 32 ~ 80V

   Vin(nom): 48V

   Vout: 24V

   Iout(full load): 4A

After confirming that the provided simulation runs without a problem,

I tried to simulate 24Vout 4Aout using the values of the parameters found in quickstart_calculator Excel file.

I modified feedback resistors, Cboot, Lout, Rrt and Rs. I added a Rboot.

   Rfb(h) 290k, Rfb(l)10k, Cboot 47n, Rs 8m, Rboot 1

When Fsw is 400KHz(Rrt 54.9k) and Lout is 22uH, it works without a problem.

However Fsw is 2.2MHz(Rrt 9.09k) and Lout is 4.7uH, a error occurs and the simulation stops

I would like to ask for advice.