Part Number: LM5156H
Tool/software:
Hi, TI expert
A customer has requested a circuit review of LM5156H applied.
Please check if there are any parts to be modified or added.
7103.POE+SWITCH_SCH_REVIEW.pdf
Please check. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5156H
Tool/software:
Hi, TI expert
A customer has requested a circuit review of LM5156H applied.
Please check if there are any parts to be modified or added.
7103.POE+SWITCH_SCH_REVIEW.pdf
Please check. Thank you.
Hi Grady,
Thanks for reaching out.
I can review the schematic. For this i need to know the design specifications (Vin, Vout, Iout).
Also it would be helpful if you can fill out the quickstart calculator for this device. https://www.ti.com/tool/download/SNVC224
Best regards
Moritz
Hello Moritz,
I will answer your inquiry.
I plan to use it with the following specifications.
Vin : 8 ~ 32V
Typ : 13.2V
Output : 50V, Max 1.2A
I do not know how to link the excel file you sent, so I am attaching the file.
Thank you.
LM5155_56_Quickstart_Calculator_for_Boost_Converter_Design_V1_1_1(DTEG).xlsx
Hi Kim,
Thanks for the additional information.
There are many things that are not matching between the values in the calculator compared to the schematic.
I assume that the schematic values are the right ones. Then i have the following points:
- The inductor saturation current is not sufficient. At min Vin, the current will go up to 8A.
- Please check the UVLO resistor divider again. At which voltage you want to stat up/shut down?
- Please check the compensation values again, the design would be unstable with the values used in the schematic.
Best regards
Moritz
Hi Moritz
Thank you for your reply.
I have reviewed the information you sent and rewritten it.
Please check.
Thank you.
Kim.POE SWITCH_SCH_REVIEW(ARROW)_20250218.pdfLM5155_56_Quickstart_Calculator_for_Boost_Converter_Design_V1_1_1(DTEG)_250217.xlsx