Other Parts Discussed in Thread: UCC14241-Q1, , UCC21738-Q1
Tool/software:
Hi,
I am trying to use the UCC14240 isolated DC/DC module to drive a pair of UCC5390S.
As far as I understand, it is possible to power the UCC5390S with a dual output voltage generated by the UCC14240.
The UCC14240 should generate the +15V and -5V voltages which power the isolated side of the gate driver.
I am now trying to specify the value of COUT3, but I can't properly interpret the meaning of the parameters listed in the component’s datasheet or how to determine them.
• I(VDD-COM) is the total current from VDD to COM, excluding average gate drive current.
• I(COM-VEE) is the total current from COM to VEE, excluding average gate drive current.
• IQ_DRIVER_VDD-COM is the maximum quiescent current of the gate driver from (VDD – COM), and any current pulled from VDD by external logic must be included.
• IQ_DRIVER_COM-VEE is the maximum quiescent current of the gate driver from (COM – VEE),
• IOther_load_VDD-COM is the maximum current pulled from VDD to COM by external logic.
• IOther_load_COM-VEE is the maximum current pulled from COM to VEE by external logic.
The preliminary schematic is shown below, any suggestions is welcome.
Best Regards,
Federico Filosomi