Tool/software:
Hi, I have been trying to simulate the online available model on the PSpice for TI software and not able to get the transient response with DC 12V input instead the model is working with pulse(0 to 12VDC) with the same configuration of the resistors on the pin of the IC. Below is the image attached of the working pulse model for the reference. Could you please help to resolve it?
Simulation Details:
Vin- 12V(DC)
Vout- 1.8V@0.7A
Switching Frequency- 2.5MHz
Transient Condition- 2.4A/230ns
Let me know if any other detail is required.