Tool/software:
I'm not seeing any information in the TPS2490 datasheet about reverse current operation.
The controller will begin to limit the gate drive to the external high side NFET when the current sense voltage is +50mV measured from Vcc to SENSE.
However, what does the controller do if it observes -50mV across the sense resistor (reverse current from load to source), or any negative voltage for that matter?
In the event of negative current sense voltage, will the controller begin reducing the NFET gate drive, in which case any continued reverse current will simply conduct through the body diode of the FET?