Other Parts Discussed in Thread: LM70840
Tool/software:
Dear TI
I am designing a circuit using a LM70880 with the following specifications.
Vin: 32 ~ 80V
Vin(nom): 48V
Vout: 24V
Iout(full load): 4A
I tried to get a reference circuit using Webench, but it didn't generate the circuit due to stability issues.
After that, I ran Webench with the above conditions without specifying the IC(LM70880).
At this time, the LM70840 circuit was generated.
Will it be difficult to use LM70880 with the above conditions?
Thanks,
Best regards,
Shinyoung Kim