Part Number: LM5148
Other Parts Discussed in Thread: LM5137
Tool/software:
Hi,
I am designing a power supply circuit with 48V input and 24V x 10A output by driving LM5148s in parallel.
The datasheet states that "dual-phase mode with accurate current sharing can be set," but how accurate can the current balance be?
For example, if the distribution of 10A is 4A and 6A, is that within the appropriate range?
For example, if it is 3A and 7A, is it unbalanced and requires some countermeasure?
Best regards,