Other Parts Discussed in Thread: EV2400
Tool/software:
Hello TI team,
When I tested the charger board under the following conditions, the IC burned.
- VBAT port : Open (not connected Battery)
- I2C : Connected EV2400 with Laptop
- Charger board : no power condition
- VAC port : is connected to a 48V DC voltage source(active) via a power supply.
The IC burned at the moment when an active 48V DC jack was connected to the charger board.
As you already know my charger board schematic, VAC line doesn't have a lot of capacitance(less than ~2uF)
This scenario (connecting an active VAC line) is a common use case, and needs to be tested repeatedly for reliability.
1. Have you seen a similar case before?
2. Do you have any suggestions for protecting input line and the IC VAC port?
Thank you.