Tool/software:
Hello there.
I have some questions regarding the previous case's responses.
Please help me answer them.
1、Does Load Mode/select = 0x81 correspond to the AVG P LAST RUN register?
2、When Load Mode/select = 0x81, is AVG P LAST RUN used for FCC and RM simulations?
3、Regarding the difference between Load select = 0 and load select = 1, my understanding is as follows:
When load select = 0, the fixed values of the existing AVG I/P LAST RUN are used for simulations. These two registers will not be updated during the discharge period.
When load select = 1, after the discharge lasts for more than 500 seconds, these two registers will be updated, and the values in these two registers will be used for simulations.
Please confirm whether my understanding is correct?
If there are any errors, please tell me the specific differences.
4、In the TRM, regarding the update conditions for AVG I LAST RUN and AVG P LAST RUN, my understanding is that:
continuous discharge (with the discharge current > [Dsg Current Threshold]) for more than 500 seconds is required.
Only after that, the average calculation of I and P will be carried out at a cycle of 1 second, and AVG I LAST RUN and AVG P LAST RUN will be updated after the discharge ends.
Please confirm whether my understanding is correct?
If there are any omissions or errors, please tell me the detailed update conditions.
5、The unit of AVG P LAST RUN is 0.1h rate. After calculating with the formula Design Capacity/(AVG P LAST RUN * 0.1), is the unit mA? Why isn't it mW?
6、If the unit of the calculated AVG P LAST RUN is mA, then how does this register simulate FCC and RM in the Power model?
Hello there, 针对之前case中的回复,有一些疑问,请帮忙解答下。
1、Load Mode/select=0x81,对应的寄存器是AVG P LAST RUN吗?
2、Load Mode/select=0x81,是使用AVG P LAST RUN进行FCC、RM仿真吗?
3、Load select=0和load select=1的区别,我的理解是:
load select=0时,使用已有的AVG I/P LAST RUN的固定值进行仿真。在放电期间不会去更新这两个寄存器。
load select=1时,放电超过500秒后,会更新这两个寄存器,并使用这两个寄存器的值,进行仿真。
请确认理解是否一致?如有错误,请告知具体的区别?
4、在TRM中,针对AVG I LAST RUN和AVG P LAST RUN的更新条件,我的理解是:需要连续放电(放电电流>[Dsg Current Threshold]),超过500秒以后,才会按照1秒的周期对I和P进行平均计算,并在放电结束后对AVG I LAST RUN和AVG P LAST RUN进行更新。请确认理解是否一致?如有遗漏或错误,请告知详细的更新条件?
5、AVG P LAST RUN的单位是0.1h rate,使用Design Capacity/(AVG P LAST RUN*0.1)的公式计算后,单位是mA吗?为什么不是mW?
6、如果AVG P LAST RUN计算后的单位是mA,那么该寄存器在在Power model下,如何对FCC、RM进行仿真?