Part Number: TPS26750
Tool/software:
Hi,
I am following the process in chapter 6.2 in TPS26750 Technical Reference Manual (SLVUCR7 – SEPTEMBER 2024) without luck.
I am using the low region binary generated from the USBCPD Application Customization tool. Is this correct?
It seems that what I try to download is not recognized as a patch. Here is the output data from the PBMc task.
Is the header "ACE0_0001" part of the bundle?
DevicePatchCompleteStatus = 0x80 and AppConfigPatchCompleteStatus = 0x40
PBMc_output:
00 00 40 80 00 05 4b c7 7a e3 3c 3b 1e f8 01 8b
35 04 19 bc 49 44 34 08 00 03 01 3a 01 1d 00 00
20 0b 98 0e 00 00 00 00
I find the documentation not very clear regarding what a bundle is, what is the configuration and what is application.
It is also a bit unclear if TPS26750 can be used without an EEPROM.
Could you also clarify the payload of the PBMs task from chapter 5.4.1? Is the payload 6bytes long? What is the number of the first byte, 0 or 1?
- What is the endianness of Low Region Binary bundle size? LSB or MSB first?
- Bundle size field is referring to bytes 0-3, while byte 1 to bits 8:15. The next field is i2c target address in byte 5.
In the Write Patch Bundle burst data stage:
- does the bundle need to be downloaded in a single I2C transaction?
- What about the Unique Address write register protocol where first byte in the transaction is the byte count to follow?
Best regards,
Georgios