Tool/software:
I am looking to use the BQ76952 battery monitor to create a HW architecture for a low cost 48V battery BMS that complies with the latest UL1973 certification requirements that, critically, does not require any safety-critical software. Is there a way to boost the diagnostic coverage of the BQ76952 using HW? Are there any ideas on using two BQ76952 for redundancy?
Can you provide recommendations or reference materials on compliant architectures? Is there a TI representative I could get in touch with directly?