This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56837: design BGA cap per ball

Part Number: TPS56837

Tool/software:

HI Ti

i read SPRABV2 General hardware design/BCB design/BGA decoupling

in page 5

15uF cap for 10 BGA power ball

i have a question

the same platform CPU have different TDP

example

intel Raptor Lake i3(35W) VS i7(125W)

the cap design is the same?

or have other design guide?

one more question

 if i design LC filter

ADCAV33 for BGA 2 ball

and use 1uF + 0.1uF for  LC filter

for the design guide "15uF cap for 10 BGA power ball"

i think it mean 1.5uF for 1 BGA,so here is need 3uF cap

before LC filter have other cap,Is it included?