Tool/software:
Hello,
I just received the Evaluation board for BQ24610EVM, and I am about to test it. I am planning to connect a DC supply up to 24V DC to Power supply #1 but I realized the port is labelled ACPWR. I wanted to ask if it is ok to connect a DC input to this port. Also, I am not planning to connect Load #2 and Power supply #2, Can i just connect a single cell 4.2V li-ion cell to Load #2?
P.S I am planning to design a single cell 4.2V lithium-ion cell charger with the chip. My charging current will be 10A and charging voltage 4.2V, input voltage to the circuit will be 24VDC. I am not going utilize the system feature so BATDRV will be floated.
Looking forward to hearing from you.
Regards,
Tee