Part Number: TPS6287B25EVM-024
Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hello,
I bought the USB2ANY and connected it to TPS6287B25EVM with 10 pin interface. I selected I2C in 'Select Interfaces' menu, entered default 0x45 in Slave Address. What do i need to enter in other parameters for enabling the I2C interface and read/write registers?
The regulator on EVM is enabled and working because I can see 0.4V at the output with 3.3V input. Do i need to switch any jumpers on the eval board to make it work with USB2ANY?
Regards,
Sanket