Part Number: BQ76952
Other Parts Discussed in Thread: BQ34Z100, BQSTUDIO
Tool/software:
Dear TI,
I have a question already posted about communicating with both a bq76952 and a bq34z100.
I explained that I tried all the tricks already posted about the issue and that it didn't work.
It would only allow me to properly talk to the bq3z4100. The bq76952 never communicated correctly.
The only way I could get it the bq76952 to work was to remove the bq34z100.
Then bqStudio would open the bq76952. However, it would open with I2C CRC communication.
I realize now that the bq7695202 has CRC enabled. I have not read up much CRC but I'm wondering if that could be causing the issues I was seeing when trying to communicate with both parts the same bus.
With the bq34z100 being I2C and the bq76952 being I2C with CRC.
I found that using the SWAP_TO_I2C command would get it just I2C.
My only familiarity with the bq76952 is using the Eval Kit which I see comes with the standard bq76952 that does not have CRC Enabled.
Any thoughts on this are appreciated.
Regards,
Kevin