This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HTC30-Q1: TPS1HTC30-Q1 Question about Max PWM

Part Number: TPS1HTC30-Q1


Tool/software:

The TPS1HTC30-Q1 datasheet specifies the maximum PWM frequency as 750Hz.

However, in other sources, the maximum PWM frequency is calculated by adding the Ton and Toff values.

TPS1HTC100-Q1: TPS1HTC100-Q1 - Power management forum - Power management - TI E2E support forums

When adding the maximum Ton and Toff values from the datasheet (200 + 230 = 430us), the resulting frequency is approximately 2.3kHz.

Why is there such a large discrepancy between the datasheet value and the calculated frequency?