This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: SOC early 0%

Part Number: BQ27Z746
Other Parts Discussed in Thread: GPCRA0

Tool/software:

I used the GPCRA0 method for learning. After completing the process, I imported the GG file and performed another charge-discharge cycle. I found that near the end of discharge, the state of SoC drops rapidly from 5% to 0%. When SoC reaches 0%, the voltage is 3.14V, but I set 0% at 3.0V.

I don't understand if there is a setting error or if there is an issue with the GPCRA0 creation. (I have recreated the GPCRA0 twice, but the problem remains the same.)



7651.gg_out.gg.csv