Other Parts Discussed in Thread: TPS631000, TPS631010, TPS631011, TPS63805, TPS61299
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Karpagadevi,
I'm sorry that I don't understand 'either or both (3.2V to 3.3V and 3.8V) and (3.2V to 1.8V)'. Can you chare Vin range and Vout target?
Best Regards,
Travis
Hi Travis,
I need Part numbers for the DC-DC Converter with 1A output current and low quiescent current and
Input voltage range: 1.5V to 4V
Output Voltage range: 1.5V to 4V
We are using the converter to convert voltage from
3.2V to 3.3V
3.2V to 3.8V
3.2V to 1.8V
With Regards,
Karpagadevi T
Hi Karpagadevi,
I am little confused, from your detailed application info, seems your input voltage is 3.2V only, but in your requirments, there is a big range? why and which is correct?
Recommend our TPS631000/TPS631010/TPS631011 for your application. altough it can not absolutly meet your input voltage range.
Regards
Tao
Hi Tao,
We are using a battery to power the DC-DC converter, which operates within a voltage range of 2V to 3.8V. Therefore, we require a DC-DC converter that supports an input voltage range of 2V to 3.8V with High efficiency and low quiescent current.
With Regards,
Karpagadevi T
Hi Karpagadevi,
Ok, it is clear here.
Recommend device mentioned above. thanks.
Regards
Tao
Hi Karpagadevi,
I am afraid TPS6310XX series is our lowest quiescent current device for your application.
Other option should be TPS6380X family. TPS63805/6/7.
Regards
Tao
Hi Karpagadevi,
Please look at TPS61299 family. The TPS612997 in TPS61299 family will be availible.
But step down operation is not supported for boost devices. Vout has to be higher than Vin.
Best Regards,
Travis