This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF6025: Requirement for output capacitor

Part Number: REF6025


Tool/software:

Hi experts,

For the output capacitor of REF6025, customer prefers two types: 22uF, 80mohm ESR electrolytic cap, or 47uF, 45mohm ESR, electrolytic cap. However, for 22uF cap, the ESR may drift to as high as 160mohm, exceeded the max requirement of datasheet. For 47uF cap, the capacitance tolerance is +/-20%, there is also risk for maximum capacitance violates the max requirement. Can anyone tell me if this concern is necessary? Which one can be used without risk?

Thank you!

John