Tool/software:
Hi,
My customer is making a mock-up of a lamp, and is trying to find the maximum power that could be dissipated on the driver. They are using 9 LEDs with a maximum Vf of 2.75 and If of 0.7A. I took an efficiency rating from the data sheet and calculated the power dissipated from that, but it appears to be too high.
Do you know what the maximum power that can be dissipated on the driver is?
BR, Ross