Other Parts Discussed in Thread: BQ25756, BQ25750, TIDA-010042, BQ25756E
Tool/software:
HI, i am trying to design MPPT charger that will be able to charge 12V or 24V LifePo4 battery packs (usually 300Ah or more).
Solar panels are from 12-50V range and input current in some cases above 40A. Batteries can be charged with 150A in CC mode so i would like to use maximum power from panels.
For now, my research on this forum was about BQ25756, BQ25820, BQ25750. Now all of them have a current limit for 20A, since i don't need reverse mode BQ25820 was the best option I found, but the problem is that in the datasheet BQ25820 and BQ25750 only do panel sweep option for MPPT tracking while BQ25756 after panel sweep is doing pertrud and observe and only has P_AND_O_TMR register.
Now my questions are
1. Am i on the right track for valid MPPT IC for my case (input: 12-50V, 40+A output:12-29V 40+A)
2. IF BQ257xx series are the way to go, am i locked to 20A current or that can be higher (putting 2 BQ chips on the board won't work since they are using the same IC2 addresses and won't work on the same solar input)
3. What about TIDA-010042 is that something i should be focusing on, but that will require MCU to calculate PWM for MPPT and it is limited to 16A but i think that can be set higher up to 35A since the driver can handle that or what should be my options. (can uC be ESP32 ?)
Chargers will be installed on the boat where solar panels are moving a lot so MPPT tracking is very important (panel sweep timer is I think 3 minutes minimum or forced and I am not sure how long it takes to scan, on some of your videos i have seen around 3-6 sec for full range).
Thank you for any advice!
Kind regards,