Tool/software:
Hi team,
If 300mA or 150mA is written to the register [Reg 05h, bit2 - 0] of the termination current and the battery is charged in the environment of 0 to 10°C, the status [Reg 00h, bit6 - 4] will be 011-Charging from IN or 100-Charging from USB, but not 101-Charging Done.
(The current is gradually decreasing with each increase in battery voltage (CV charging), but the status does not become 101-Charging Done at the set end current value.)
*This phenomenon does not occur under normal temperature.
Is there any possible cause?
Best Regards,
Ryu.