Tool/software:
Hi Team,
I'm planning on build a high-side switch with LM74502. But can I drive EN with PWM(250-300Hz)? as I want the switch to have PWM output capability.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shiven,
Just read that on section 9.4 it uses OV pin as logic input, whereas I feel the inverted PWM is not desireable since I will need a spare GPIO to control the EN pin as master switch to temporary turn off the device before the inverted PWM is available otherwise if I just tie EN to VS it would turn on itself whenever the power is on and the inverted PWM signal is not pulled up. If EN pin can be PWMed as well, should I just tie OV into GND? With resistor or without?