Tool/software:
We are developing a Buck-Boost Converter using LM5176 and using reference from SNVC208
Following are specs of the design:-
Vin:- 6 to 51V
Vout:- 12.2V
Iout:-15A
Switching Frequency:- 440 kHz
We need help with reviewing the schematic as well as the PCB board for the same. Will share the files on private chat.Please do send me a friend request so that we can continue chat.
Please do look into the schematic and PCB and let me know if there are any changes to do.
Thanks & Regards
Vinay Mande