Other Parts Discussed in Thread: UCC28C42
Tool/software:
I have generated the offline flyback converter design report from TI WEB Bench Power designer tool for following specifications .

As per the design report , turns ratio is Np/Ns= 64/7 =9.14 and magnetizing inductance is Lm= 378uH .
UCC28750 datasheet also has design procedure explained in detail .
by referring equations 6,7,8 and 9 from design procedure
Turns ration comes out to be 16.:1 and Lm =2mH for Vbulk_min =109V , DMax =0.65 , Vout=12V , Iout=5A , n=80% , Kccm= 0.166
values of turns ratio and magnetizing inductance are not matching to web bench report .
Is it incorrect to use datasheet formulas to determine the aforementioned parameters?
please advise .