This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562208: TPS562208

Part Number: TPS562208
Other Parts Discussed in Thread: TPS564252

Tool/software:

Hi,

I have a 9V battery and I need to step down voltages to 3.3V for a MCU, Sensor and a motor driver. I am expecting 2A max load current.
I need a efficient, small size as possible and cost effective solution for it. It would be great if it is fixed output solution and I am more leaning towards buck converter to keep efficiency high unless there is some other options available.
If it has overvoltage, under voltage feature. It would be great but not necessary.
Can you help me with it plz?

Thanks