Tool/software:
Hello,
The FAQ says the to program the OTP one need disconnect all cells from the device.
I do i need to physically disconnect them or i can simply set Vcell Mode register to 0.
Thanks
Vadim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
The FAQ says the to program the OTP one need disconnect all cells from the device.
I do i need to physically disconnect them or i can simply set Vcell Mode register to 0.
Thanks
Vadim
Hello Vadim,
In order to program OTP, 10-12V must be applied to the BAT pin and the highest VCx pin. This usually means physically disconnecting the battery cells to allow for this.
Vcell mode just allows the protections for those cells to be disabled so they don’t prematurely trigger protections. More information on Vcell mode can be found in Section 13.3.2.19 Settings:Configuration:Vcell Mode from the technical reference manual.
Best Regards,
Alexis