This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28750EVM-071: Request for information about a circuit that inputs AC single-phase 220V and DC 9~24V Volt (MCU Control).

Part Number: UCC28750EVM-071


Tool/software:

Do you have information on purchasing a 200W development board that inputs AC single-phase 220V as input power and outputs DC 9~24V voltage (MCU control)? 
(It is okay if the output power is lower than 200W) If you can receive technical support in Korea, please also provide the relevant contact information.