This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: OV pin max leakage current; Vovr value (Datasheet clarification)

Part Number: LM7480-Q1

Tool/software:

Hello,

I'm calculating UVLO and OVLO resistor values and stumbled upon some differing values in the datasheet.

Leakage current in OV pin:

  1. DS chapter 7.5: I(OV): 53nA(typ) / 200nA(max)
  2. DS chapter 10.2.3.5 / 10.3.2.4: „Maximum leakage current into the OV pin is 1 µA"

--> Which value is correct - 200nA or 1µA?

V(OVR):

  1. DS chapter 7.5: 1.195V(min) / 1.231V(typ) / 1.267V(max)
  2. DS chapter 10.2.3.5: „Based on the device electrical characteristics, VOVR is 1.23V“
  3. DS chapter 10.2.3.5: „Based on the device electrical characteristics, VOVR is 1.233V“

--> I would assume 1.23V for simplicity, but anyway - which value is correct?