This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24612: The auxiliary power supply design issue for UCC24612

Part Number: UCC24612
Other Parts Discussed in Thread: TIDA-00702, UCC28740,

Tool/software:

Hi,

We has a new design for the auxiliary power supply, and our spec. for below:

1. We need to auxiliary power supply output is 24V/3.3A(fully loaded);

2. The output use the synchronous rectification UCC24612-1DBVR solution, the QR Flyback solution use the UCC28740DR+CS6N120( 6A1200V MOSFET);

Our issue is the below:

1. The switch frequecy is still work on 43K-55KHz when the fully loaded(3.0A+0.3A), and the MOSFET will be enabled at several waveform valleys, we can not increase the switch frequency,

2. Half Load/ Light load, the switch frequency will be 20K-30KHz, we can hear the Inductive whistling sound;

3. The efficiency is about 87%, and the EVM is more than 90%;

Our support need:

1. We need to Increase the switch frequency to 50K~55KHz and the MOSFET will be enable on the first waveform valleys;

2. How to modify our design that we can limit the switch frequency more than 30KHz if it is on different load;

3. We test design based on the TIDA-00702 EVM: R28 to 200K, R30 to 10-20K and there are no improve:

We test the waveform for your evaluated:

1. Vds waveform:

2. Vin=250VDC, output current=3.3A:

3. Vin=310VDC

The transformer file and schematic diagram please refer to below

PQ3220P12M420U.pdf

PQ3220P12M420U (2).pdf

  • Hello Zhang, 

    This issue is related to design parameters related to UCC28740 controller.  It cannot be solved with changes involving the UCC24612 device. 

    Please submit a new E2E thread with all this same information, but change the part numbers in the thread title to "UCC28740".

    That will alert the correct team within TI to address your issue. 

    I will close this thread, please resubmit with the new part number in the title. 

    Regards,
    Ulrich

  • Hi Ulrich,

    Thanks, I have created a new thread for this issue, thanks.