Tool/software:
I have a question about circuit design
1. To use OUTH1,2 / OUTL1,2, GD2, GD1, and GD0 will be set to 1, 1, and 0 respectively when the inverter is running. And I will change GD0 to 1 only during Fault Reset.
In this case, is it okay to always fix GD2, 1 pin as pull-up?
2. I'm not going to use SPI communication. I want to get a fault signal by tying up the Fault n1, n2 pins and connecting them to the DSP. Is this possible?