Tool/software:
Hi
I understand that adding Cff is an option.
However, when designing other dc-dc, he said that Cff should be added when it is above a certain output voltage.
Should TLV758p also add Cff depending on the output voltage?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi
I understand that adding Cff is an option.
However, when designing other dc-dc, he said that Cff should be added when it is above a certain output voltage.
Should TLV758p also add Cff depending on the output voltage?
Thanks
Hi David,
There isn't necessarily an output voltage dependence for the feedforward capacitor on the TLV758P. If large resistor values (>500kΩ, for example) are used in the feedback network, transient response and PSRR may be degraded due to the feedback resistors interacting with parasitic capacitance from Vfb to GND. Adding a feedforward capacitor helps compensate for the parasitic capacitance, improving transient response and PSRR.
Best Regards,
Alex Davis