This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552872-Q1: 芯片损坏

Part Number: TPS552872-Q1

Tool/software:

Hi TI team

 

我们的PCBA在进行FCT测试的时候,出现了4pcs TPS552872QWRYQRQ1芯片损坏的问题

 

目前检查了其中两颗芯片,失效状态如下:

1)芯片1失效状态(板上测试:①VINPGND阻值0.4Ω、②SW1PGND阻值0.4Ω、③SW2PGND阻值0.4Ω、④VOUTPGND开路、⑤VOUTSW2开路、⑥VCCPGND阻值10.2Ω)

2)芯片2失效状态(板上测试:①VINPGND开路、②SW1PGND阻值0.5Ω、③SW2PGND阻值0.5Ω、④VOUTPGND开路、⑤VOUTSW2开路、⑥VCCPGND阻值10.4Ω)

3)芯片2失效状态(裸片测试:①VINPGND阻值16MΩ、②SW1PGND阻值0.5Ω、③SW2PGND阻值4.6MΩ、④VOUTPGND开路、⑤VOUTSW2开路、⑥VCCPGND阻值10.4Ω)

电路设计参考手册TPS552872-Q1 汽车类 36V 4A 完全集成式降压/升压转换器 datasheet 中7.2 Functional Block Diagram

可以帮忙分析一下可能导致失效的原因是啥吗?

  • Hi Jimi,

    Thank you for reaching out. What is the application and project here?

    Can you describe during what kind of test, the device fails? Start-up or steady state? In factory or OEM?

    Can you provide schematic and layout to check if there is any design problem? What is input voltage range, output voltage and output current. What is the part number of output caps. What is saturation current of inductor?

  • Hi Jimi,

    Since we have discussed it with FAE, I will close this thread now.

    If there is still something open, please reply and the thread will get opened again.
    If you have any other question or of the thread has been locked, please open a new one.
    Clicking the Resolved Button also helps us to maintain this forum.

    Regards,

    Mulin