This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51770: Interface forum

Part Number: LM51770
Other Parts Discussed in Thread: LM5177

Tool/software:

Hi TI experts,

I intend to use this chip to design a power converter that can be integrated with a LiPO battery as one single energy storage system solution. Please see battery specs below:

Input voltage range: 10V - 16V

Output voltage: 13.8V - 14V

Power: ~200W

Therefore:
In the forward direction, the battery supplies a system load of regulated 13.8V - 14V through the power converter.
In the reverse direction, the battery can be charged (from 20% SoC @10V to 90%SoC @16V) with a smart charger / DC power supply through the power converter. 

I have several questions on the implementation:

1. The forward direction implementation is clear. However for the reverse direction, what must be done so that battery overcharging is prevented?

2. I intend to implement a 10mF output bulk capacitance to meet system load requirements. In the forward direction, soft-start reduces the in-rush current of the output capactior. However, how can the inrush current be limited in the reverse direction? This is to protect the smart charger / DC power supply.

3. I noticed in the quickstart calculator tool, the crossover frequency and phase margins are explicitly stated in the graph. It seems like the gain margin is not a priority for this chip. May I ask what is the reason for this?

4. In terms of my application, would LM51770 or LM5177 be better?