This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8865Z-Q1: Max. output current when using PWM

Part Number: LP8865Z-Q1


Tool/software:

We will use the LP8865 in our product; we will set ADIM to 100% and use PWM at 30Hz with a 2ms on duty time.

I would like to ask: The datasheet states ‘Up to 2-A output current in buck topology,’ does this mean constant current?
Can I set a higher current value in PWM mode? Is the limit only up to the CURRENT LIMIT (ILIM)?"