This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2040: BQ2040

Part Number: BQ2040


Tool/software:

Having trouble with the voltage calibration.   The application is a Li-ion 7 cell at 4 V per cell = 28V.   Page 3 of the datasheet describes the in-circuit resistor values  in Chart 1 only to 4 cells.  How are the values derived for this application with 7 cells?    The design is using a D5 = 4148 diode with a Q1= 2N7002 MOSFET in the Vcc input with R11= 2 Meg ohms  R5= 1.4 Meg ohms, R4= 100K  to get  divider ratio of 15 to 1.

.

  • Hello,

    The BQ2040 is not specifically designed for direct multi-cell monitoring or management in a 7-series (7S) Li-Ion configuration. It’s a fuel gauge IC that tracks capacity via coulomb counting and communicates over SMBus, typically working with an external microcontroller or battery management system (BMS) for multi-cell setups. To configure it for a 7S Li-Ion battery pack, you’d need additional hardware (e.g., a cell monitoring/protection IC) and careful software setup.

    The BQ2040 isn’t ideal for a 7S configuration due to its age and limitations. For a 7S Li-Ion pack, consider a modern alternative like the BQ41z90