Other Parts Discussed in Thread: BQ24172
Tool/software:
From the TI Application Note "LiFePO4 Design Considerations" the BQ25798 is said be a good choice for a LiFePO4 battery. However, looking at the BQ25798 datasheet( BQ25798 I2C Controlled, 1- to 4-Cell, 5-A Buck-Boost Battery Charger with Dual-Input Selector, MPPT for Solar Panels and Fast Backup Mode datasheet (Rev. B)) I am not so sure anymore.
Is it indeed suitable for LiFePO4 batteries?
So, What happens when the battery is completely empty? Registers are reset and by default it charges autonomously with Li-Ion voltages which are too high for LiFePO4? Charging will never reach the end voltage, does it stop charging at some point or is there a serious risk involved? If that happens incidentally, how does it affect the lifetime of the battery (can it be acceptable for very low occurrences)? The registers can only be set when the device is manually turned on, not while charging.
It's intended purpose is for a portable medical device with a 2 cell 2200mAh LiFePO4 battery via USB-C. The device does not start automatically when charging, it needs to be turned on separately and it is also not supposed to be used while charging. So no BQ25798 registers can be set when charging from completely empty, it is used in autonomous mode.
Thanks for helping out!