Other Parts Discussed in Thread: TLV1117, TLV1117LV33EVM-714,
Tool/software:
Hi Experts,
Could TLV1117LV33EVM-714 be directly used to verify TLV76133's performance? Thanks.
BR,
Skylar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Experts,
Could TLV1117LV33EVM-714 be directly used to verify TLV76133's performance? Thanks.
BR,
Skylar
Hi Skylar,
Do you mean using the TLV1117 that is populated on the TLV1117LV33EVM-714 to validate the TLV761? Or do you mean to populate a TLV761 on the TLV1117LV33EVM-714? These devices have different dies so using a TLV1117 to validate the TLV761 will not work. If you are asking if the TLV761 can be put on the TLV1117LV33EVM-714, then yes the pinout for the DCY packages is the same so that can work.
Regards,
Nick
Hi Nick,
I mean that populate a TLV761 on the TLV1117LV33EVM-714 as I need a EVM to test TLV761. Thanks for your clarification.
BR,
Skylar