Tool/software:
I was wondering if I could know through GPIO which sink PDO the TPS25751 operating in sink mode has contracted with the source device.
The system I am designing is power amplifier and TPS25751 is used only sink mode.
I would like to change output power level by contracted watt with source device.
I wonder that one of some solution is uCOM read register of TPS25751. ( Is that correct ? ), but I would like to avoide digital noise
as much as possible, so I don't want to select i2c.
Is it possible to know through GPIO which sink PDO or which watt the TPS25751 operating in sink mode has contracted with the source device ?
Sincely yours,