Tool/software:
Hi,
I have manufactured 100pcbs having LP3982ILD-3.0/NOPB as an LDO converting LiPo battery (3V-4.2V range) to a 3V output. For 25pcbs the output was fine. Rest 75 were kept in factory within ESD safe sheet for about an year for later use. The battery was disconnected from this LDO as the switch was kept off (Switch disconnected the connection from battery to LDO input). Few days ago we started manufacturing process again and changed the older LiPo to a new one with same MPN (3.7V nominal V, 600mAh).
By testing first 10pcbs for LDO voltage output, it turn out to be 3.3V instead of 3V. Generally when this happens, according to my experience, the LDO gets heated up or when a load is connected the voltage drops drastically. But in this case none of these happened. The circuit is working fine with load. My load is an ESP32 controller which is safe to work at 3.3V also.
My questions are:
1. Why is this happening if datasheet says 2% error in output voltage? I have purchased this IC from ti.com -- official TI website
2. Now if it is giving 3.3V and rest of the circuit is working fine (since circuit has 3.6V max limit) can I proceed forward for integrating this PCB in my product? I am dicey about the longevity of this IC, will it survive at least 1yr provided there is no direct contact with human on circuit in final device?
Please help me in this doubt as it may affect a serious decision in manufacturing bulk devices and saving costs.
Thanks
Swapniil