This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62A04B: Load Transient response with Oversized inductor (1µH)

Part Number: TPS62A04B

Tool/software:

Hi,

 

I had to place 1uH Buck converter section of the schematic (to facilitate alternate MFR IC drop-in replacement), even though recommended value is 220nH. This is to include alternate MFR Buck IC's inductor value. Inductor value for “TPS62A04BDRLR” is now 1µH instead of recommended 220nH.

Question: Will there be any issue prevalent in this design? Specifically Load transient response & output stability.