This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25071-Q1: BQ25071

Part Number: BQ25071-Q1
Other Parts Discussed in Thread: BQ25071

Tool/software:

Hello,

I am using the BQ25071 charging IC to charge LiPO4 battery, along with the BQ29716 as the current-voltage protection IC. Please find the charging circuit schematic here: Battery Charging Circuit.

I have observed that the battery charges with ~100 mA charge current, which should be charged using 1 A charge current. The battery used has 300mA capacity. Though the max battery charging capacity is 4.1V, the circuit stops the charging at 3.5V battery voltage.

Important note: I have to always keep Battery NTC pin disconnected in order to charge / discharge the battery. 

Battery Specification 

What changes I need to do in order to charge the battery at 1 A charge capacity also charge it up to 4.1V.

Thanks,
Sagar