This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36506-Q1: output back feed

Part Number: LMR36506-Q1

Tool/software:

Hi,

I use LMR36506-Q1 as Vbus (5V) generation for USB2.0 OTG application

VIN =12V

Vout=5V

;;;; Vout connect to USB connector Vbus

when we plug the USB to the computer which is host, we noticed that VIN = Vout when VIN has not applied.

Question: will this back power damage the LMR36506-Q1?

Thanks