Other Parts Discussed in Thread: TPS54302
Tool/software:
Good day,
I am currenlty designing a product that needs to have a stable 3A 5V output from a supply ranning from 5V up to 24V.
Part of this supply will be coming from a USB-C PD power supply, and im strugging to see how to achieve a 5V supply when the source voltage is 5V. The current regulator we have been using from a competitor needs at least 6V to achieve a stable 5V output, which is not really feasable with a 5V USB source.
Would a buck regulator such as the TPS54302 with 100% duty cycle be the way to go, though i believe the low frequency would require a larger inductor. But the buck regulators that can go multiple Mhz dont look to be able to achieve 100% switching, such as the TPS62933
Any advise for a suitable power regulator would be greatly appreciated.
Is there any guidance on designing a Multi power source USB-C PD device that can handle voltages from 5-20V@~3A
Kind regards
Ben J